1 … 272 273 274 275 276 … 364 2740 / 3635 POSTS

What is the physical layer?

* Question What is the physical layer? * Answer The WirelessHART physical layer is basically based on the IEEE 802.15.4-2006 2.4GHz DSSS phy [...]

What are the main reasons for the difference in sensor nodes between time points in sensor networks?

* Question What are the main reasons for the difference in sensor nodes between time points in sensor networks? * Answer The initial time at [...]

What is the SCART interface

* Question What is the SCART interface * Answer SCART is an interconnection interworking interface mandated by Europe to complete satellite [...]

Classification of power electronics

* Question Classification of power electronics * Answer According to the control capability of the device, it can be divided into the follow [...]

What is a charge pump?

* Question What is a charge pump? * Answer The charge pump is a non-radiative boost device that uses a capacitor as an energy storage device [...]

What is the latest and simplest solution for voltage monitoring and timing issues?

* Question What is the latest and simplest solution for voltage monitoring and timing issues? * Answer The newest and simplest solution is t [...]

What is the optical system of a medical carbon dioxide analyzer?

* Question What is the optical system of a medical carbon dioxide analyzer? * Answer The optical system of the medical carbon dioxide analyz [...]

What are the configurations supported by ByteBlaster II?

* Question What are the configurations supported by ByteBlaster II? * Answer AS mode: Altera's AS serial configuration chip (EPCS series) ca [...]

What is working bandwidth?

* Question What is working bandwidth? * Answer It means that the repeater is in the actual work, and does not maintain the same gain in the [...]

What are the advantages of PTN technology?

* Question What are the advantages of PTN technology? * Answer Suitable for all kinds of coarse and fine particle services, end-to-end netwo [...]
1 … 272 273 274 275 276 … 364 2740 / 3635 POSTS