1 … 274 275 276 277 278 … 364 2760 / 3635 POSTS

What are the main modulation methods used in RFID systems?

* Question What are the main modulation methods used in RFID systems? * Answer There are usually three modulation methods used in RFID syste [...]

What are the performance of WOLED?

* Question What are the performance of WOLED? * Answer 1.Color quality, the color quality of WOLED is mainly represented by CIE chromaticity [...]

What are the specific factors that are unique to RFID technology?

* Question What are the specific factors that are unique to RFID technology? * Answer • Application system configuration: hardware configura [...]

For the CBD, the development process is done by six roles. What are they?

* Question For the CBD, the development process is done by six roles. What are they? * Answer (1) Component developers are also component su [...]

How to calculate the equivalent capacitance of the transmission line?

* Question How to calculate the equivalent capacitance of the transmission line? * Answer From the information of the title, two pieces of i [...]

What is a piezoelectric crystal?

* Question What is a piezoelectric crystal? * Answer There is a very interesting kind of crystal that produces different charges at both end [...]

What are the ways to reduce interrupt latency through software handlers?

* Question What are the ways to reduce interrupt latency through software handlers? * Answer There are two ways to shorten the interrupt lat [...]

What are the types of sensors for electronically controlled in-line pumps?

* Question What are the types of sensors for electronically controlled in-line pumps? * Answer (1) rack position sensor (2) injection adva [...]

Briefly describe the working principle of the DS11-2 elevator load cell?

* Question Briefly describe the working principle of the DS11-2 elevator load cell? * Answer DS11-2 elevator load cell and permanent magnet [...]

What are the inverter operation control functions?

* Question What are the inverter operation control functions? * Answer 1.Starting frequency 2.Adding and decelerating time 3.Jog operati [...]
1 … 274 275 276 277 278 … 364 2760 / 3635 POSTS