1 … 330 331 332 333 334 … 374 3320 / 3738 POSTS

What is the main reason for the mechanical lag?

* Question What is the main reason for the mechanical lag? * Answer After the strain gauge is subjected to mechanical strain, residual defor [...]

What are the advantages of NiosII’s implementation of embedded systems?

* Question What are the advantages of NiosII's implementation of embedded systems? * Answer 1.The Benefits of a Configurable Soft Core Embed [...]

What are the restrictions on stop mode?

* Question What are the restrictions on stop mode? * Answer When all of the following four conditions are met, if the CMl0 bit of the CM1 re [...]

What is the role of the phosphorescent photosensitizer?

* Question What is the role of the phosphorescent photosensitizer? * Answer The role of the phosphorescent photosensitizer is to allow the t [...]

What are the important technical indicators of the successive approximation analog-to-digital converter?

* Question What are the important technical indicators of the successive approximation analog-to-digital converter? * Answer 1) Resolution, [...]

What is the complement/reverse command?…

* Question What is the complement/reverse command?... * Answer In digital electronics, the complement or reverse operation usually means inv [...]
VBUS054CD-FHI-GS08 Protection Device

VBUS054CD-FHI-GS08 Protection Device

The integrated circuits and microchips used in the modern electronic devices are very sensitive equipment. The phenomenon of Electrostatic Dischar [...]
PI2EQX4401DZFEX Repeater/Equalizer

PI2EQX4401DZFEX Repeater/Equalizer

PCI Express is a high-speed serial bus expansion standard which is widely used in computer motherboards. The PCI Express stands for Periph [...]
KSC3503ESTU Transistor

KSC3503ESTU Transistor

The invention of the Silicon transistors in the mid 50s is regarded as the greatest invention of the 20th century. The semiconductor trans [...]

What are the two principles of oscillation blocking?

* Question What are the two principles of oscillation blocking? * Answer The first type consists of four parts of the criterion; the second [...]
1 … 330 331 332 333 334 … 374 3320 / 3738 POSTS