1 … 367 368 369 370 371 … 373 3690 / 3726 POSTS

What is the analog output type liquid level sensor used for testing?

* Question What is the analog output type liquid level sensor used for testing? * Answer Fuel tank fuel quantity [...]

What are the components of ion selective electrodes?

* Question What are the components of ion selective electrodes? * Answer The ion selective electrode is usually composed of an electrode tub [...]

What is active power?

* Question What is active power? * Answer Active power - also known as average power.The instantaneous power of the alternating current is n [...]

What is an IC card?

* Question What is an IC card? * Answer The IC card is a combination of ultra-large-scale Integrated Circuits(ICs) technology, computer tech [...]

What are the applications of the GPRS module?

* Question What are the applications of the GPRS module? * Answer Mainly used in wireless data transmission, wireless POS, security, lottery [...]

What technologies are generally used in the preparation of POLED films?

* Question What technologies are generally used in the preparation of POLED films? * Answer The preparation method of the POLED film general [...]

What are the causes of black spot formation?

* Question What are the causes of black spot formation? * Answer (1) The thermal effect of the organic functional layer of the device, the t [...]

What are the characteristics of the Samsung S3C2440A processor?

* Question What are the characteristics of the Samsung S3C2440A processor? * Answer The outstanding feature of the S3C2440A is the processor [...]

What clock input modes can each programmable register work with?

* Question What clock input modes can each programmable register work with? * Answer 1) Global clock signal.2) The global clock signal is en [...]

What is the working procedure for the master device to manage all the power supplies on the PCB?

* Question What is the working procedure for the master device to manage all the power supplies on the PCB? * Answer 1 Class 1: The master w [...]
1 … 367 368 369 370 371 … 373 3690 / 3726 POSTS