* Question What conditions should the CPU respond to interrupts? * Answer (1) An interrupt source issues an interrupt request; …
* Question What are the important parameters in serial communication? * Answer The most important parameters for serial communication are…
* Question What are the ultrasonic probes? * Answer Ultrasonic probes are piezoelectric, magnetostrictive, electromagnetic, etc., and ultrasonic sensors for…
* Question What are the characteristics of the PCA82C250/251? * Answer (1) Fully compliant with IS0 11898; (2) High rate…
* Question Why do you have sequential execution statements in Verilog? * Answer There are two reasons. The first is…
* Question What is a cold reset? * Answer Cold reset: When the power supply voltage and other signals of…
* Question What is the independent luminescent material method? * Answer The independent luminescent material method is also called R,…
* Question What is NVRAM? * Answer NVRAM (non-volatile RAM) does not lose information after the power is turned off.This…
* Question What are the shift instructions? * Answer The shift operation includes the following six types, LSL, ASL, LSR,…
* Question What is the analytical redundancy method? * Answer Due to the popularity of computers and the powerful role…