1 … 266 267 268 269 270 … 365 2680 / 3644 POSTS

What are the common sensor interface circuits?

* Question What are the common sensor interface circuits? * Answer Impedance matcher, bridge circuit, amplifier circuit, switch output circu [...]

What are the external terminal parts of the PLC and what is the function?

* Question What are the external terminal parts of the PLC and what is the function? * Answer External terminals include PLC power terminals [...]

What peripheral register space is included in the register map?

* Question What peripheral register space is included in the register map? * Answer Peripheral Architecture 0: Peripherals that map directly [...]

What is the control channel used for?What can be divided?

* Question What is the control channel used for?What can be divided? * Answer The control channel is used to carry signaling or synchronizat [...]

What is the hierarchical structure of the frame memory?

* Question What is the hierarchical structure of the frame memory? * Answer The frame memory of each preview output port (P-port) and video [...]

What is a directional connection point?

* Question What is a directional connection point? * Answer When the vertical shaft is oriented, the measuring point is connected to the poi [...]

What are the characteristics of PID control?

* Question What are the characteristics of PID control? * Answer PID control has become one of the main technologies of industrial control b [...]

What are the performance indicators of automotive sensors?

* Question What are the performance indicators of automotive sensors? * Answer Accuracy specifications, responsiveness, reliability, durabil [...]

How to measure the quality of the triode

* Question How to measure the quality of the triode * Answer (1) Check the two PN junctions of the triode.Let us take the PNP tube as an exa [...]

In order to ensure the stable and safe operation of the system and minimize the loss caused by the fault, what are the protection measures of the control system?

* Question In order to ensure the stable and safe operation of the system and minimize the loss caused by the fault, what are the protection measur [...]
1 … 266 267 268 269 270 … 365 2680 / 3644 POSTS