* Question Which two transport protocols does the IC card support? * Answer The IC card supports two transport protocols:…
* Question What are the devices installed in the general architecture of the PLC access system? * Answer (1) The…
* Question What should I pay attention to when using Altera’s configuration chip? * Answer Make sure the configuration chip…
* Question What is the difference between the Thumb instruction set and the ARM instruction set? * Answer The Thumb…
* Question What are the main operating frequencies of RFID systems? * Answer Low frequency, 125 ~ l34kHz; high frequency,…
* Question What are the two types of reset? * Answer Reset has two types: cold reset and warm reset.
* Question Stacked silicon interconnect technology problem answer * Answer The 3D packaging method, called “stacked silicon interconnect technology,” uses…
* Question What are the power management features in some DSP devices? * Answer Including the following aspects.Reduced operating voltage:…
* Question What are the characteristics of the VxWorks operating system? * Answer 1 Reliability Operating system users want to…
* Question Briefly describe the basic components of a transmitter? * Answer (1) Modulator: As its name suggests, this component…